2021-02-11 7:49 AM
I use Nucleo-H743ZI and want use the Aduino-Header. On Board MB1137 PIN D10 (CS) is conneted to PD14. In CubeMX SPI1 NSS1 is set to PA4. I can not change to PD14, because there is no SPI1_CS in PD14 in CubeMX. How can I fix this?
I don't want change the source code after every generate.
2021-02-11 8:13 AM
Hi @Grisby ,
Thank you for these details.
Could you share your .ioc file to check this issue ?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.