2019-10-24 12:48 AM
Hi,
DMA does not work, because the initialization order of the code generated by CubeMX is not correct.
DMA setting is not valid, because DMA is initialized after the fuction that uses DMA.
Please fix bugs.
Best regards,
incorrect order expample:
MX_GPIO_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_SPI3_Init();
MX_UART4_Init();
MX_UART5_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
MX_DMA_Init();
correct order expample:
MX_GPIO_Init();
MX_DMA_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_SPI3_Init();
MX_UART4_Init();
MX_UART5_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
My environments:
・STM32CubeMX Ver. 5.4.0
・STM32Cube MCU pacage for STM32L4 Series Ver1.14.0
・Windows10
・NUCLEO-L496ZG
2019-10-24 1:11 AM
Hello,
The initialization order can be changed directly within STM32CubeMX, just go in the "Project Settings" tab, "Advanced Setting: section.
In the table "Generated Function Calls", you can select each line and thanks to two buttons at the bottom of the window, you can increase or decrease the rank of each function call.
2019-10-24 1:38 AM
Hello @TSuzu.424 ,
Thanks for your feedback, this issue has already reported and it will be fixed in a next release.
Best Regards,
Khouloud
2019-11-09 3:29 AM
Hi All
Problem is also exist for STM32F745.
Regards,
2019-12-28 1:43 AM
This bug exists in STM32F405RG with STM32CubeMX 5.4.0
2019-12-28 2:18 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.