2017-02-16 7:44 PM
Hi! I'm using Linux x86_64 with OpenJDK 64-Bit Server VM (build 25.71-b15, mixed mode). The versions affected: 4.19.0, 4.18.0
When I start STM32CubeMX and create a project, everything is fine. But if I click the 'Clock Configuration' tab, the whole X11 session freezes.
Please drop me any idea how to get more info: traces, debug, anything?
#cubemx2017-02-28 9:28 AM
For my curiosity, I tried to find an iso image. But I haven't found it.
But I am thinking that Cube is running in a java virtual machine context.
Thus if an error, or hang, occurs, it should be visible by logging java VM logs.
Just for test, you can try with Oracle java instead of openJDK.
Kind regards
Sirma
2017-02-28 6:01 PM
FWIW, I use Linux (Fedora versions, currently 24) and have never had this problem. This seems distribution specific. I do agree about putting the STM32Cube folder under
$XDG_DATA_HOME.
2017-02-28 10:54 PM
Anyway I made a new log with sending SIGQUIT to Java VM. Hope it'll help.
________________ Attachments : cubemx.log.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hys3&d=%2Fa%2F0X0000000bDO%2FcnZMLHqHOH88pd1XX4qV7D1PCBR8TSUt.tGM1nULac0&asPdf=false2017-02-28 11:36 PM
hi, Sirma!
the ISO images (Live, also can install) are here:
https://en.altlinux.org/Starterkits&sharpmain
I hoped you could advise me how to trace a Java program when it hangs like this. Or get a backtrace on signal or alike.
I would probably try Oracle java but later.
Thanks.
2017-03-01 1:11 AM
Have you tried with Oracle Java instead of OpenJDK ?
CubeMX wouldn't be the first quasi-commercial application to fail with the latter.
I guess ST doesn't validate Cube against every possible Linux distribution / Java engine combination.
2017-03-01 1:39 AM
I guess ST doesn't validate Cube against every possible Linux distribution / Java engine combination.
I didn't expect anything like that. And I don't blame ST for this non-working combination. I just humbly asked for help for my particular situation.
And hope that either I get enough info to bugreport to my distro OR help find a pitfall in CubeMX that causes that.
2017-03-01 2:29 AM
Hello Ildar,
Thanks for the log, but it does not give any clue on what could goes wrong.
By reading it more in detail, it seems that the application is installed on a network drive (/mnt/public/win-apps/STM32CubeMX).
Do you confirm it ?
If this is the case, and for test purpose only, could you install cube on your local drive and redo the test ?
(download the installation zip and run 'java -jar <path/SetupSTM32CubeMX-xxx.exe', then select a local path)
Kind regards
Sirma
2017-03-01 3:36 AM
I didn't expect anything like that. And I don't blame ST for this non-working combination.
Me neither. This would be quite a lot of work, and initial hardware investment for test platforms.
But switching Java engines is not so tedious, perhaps it gives you a running application.
2017-03-01 4:19 AM
Sirma,
the /mnt/public is not a network drive.
2017-03-01 6:07 AM
Not quite sure about your configuration.
Do you run your Linux in a VM, and is
/mnt/public
perhaps a folder shared between host and VM ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.