2025-12-16 4:42 AM
The CubeMX 6.16.0 is able to generate a CMake-project for an STM32H7 - great. A small conflict currently exists in the following two generated files [for a "basic" STM32H7 project]:
- CM7/CMakeLists.txt:69
# Add linked libraries
target_link_libraries(${CMAKE_PROJECT_NAME} PRIVATE
# Add user defined libraries
)- CM7/mx-generated.cmake:81
# Add libraries to the project
target_link_libraries(${CMAKE_PROJECT_NAME} ${MX_LINK_LIBS})
The first specifies
PRIVATEwhile the second does not - which is incompatible as per CMake.
Can someone confirm this observation?
Can this be made consistent in the future? If so, I would prefer the one with the scope keyword - but could also live without it here.
2025-12-16 4:44 AM
The same also holds for the CM4 code...
2025-12-16 5:06 AM - edited 2025-12-18 8:14 AM
Hello @JohannesWilde
Thank you for bringing this up!
This matter has been raised internally, and it is under review (Ticket 223868 This is an internal tracking number and is not accessible or usable by customers).
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.