2015-05-21 1:59 AM
In the CubeMX software, its impossible to configure 13 Bits for address lines (Row bit number). Although the define is existing in the FW library.
#fmc #stm32f4 #cubemx #sdram2015-05-22 3:07 AM
Hi Michael,
To be able to configure 13-bit row for used SDRAM, you have to set the ''Address'' for selected SDRAM (Ex: SDRAM 1) to it max value (13 bits) in the Pinout tab.Then, in Configuration tab (FMC configuration), you can select ''13 bits'' as ''Row bit number''.Hope it is clear now.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-06-29 2:27 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.