2021-07-20 6:30 AM
I actually have a Nucleo and a custom board. They are running same software and are very identical in terms of hardware but not identical: but there is at 2 pins that need to be changed and UART added: set baud rate, set NVIC IT. I also have to insert my IT handler once CUbeMX updated files (in stm32xxx_it.c)
I wonder if i could handle 2 differents layout (via ie a new target or a new board, as mentionned in CubeIDE), but i have no idea how to support this.
I guess i should have 2x .ioc files, and eventually a couple of scripts to start CubeMX generation and copy/paste the IT callback (although it coudl overwrite CubeMX generated file).
Any idea on how to do this ? Thank you !
2021-11-16 2:15 AM
Hello @DaDude
Thanks for your post,
Do you mean that you want to debug 2 projects on the CubeIDE at the same time?
Khouloud
2021-11-16 2:37 AM
hello @Khouloud ZEMMELI
No. I have a custom board and a nucleo. With the same codebase, i'm forced to change .IOC to match the hw layout (slightly different), everytime i'm switching from one to another.
I should be able to tweak this with a bunch of preprocessors #define #if but thus i'm forced to never regenerate code from cubemx if i want to keep theses changes.
2021-12-07 12:13 AM
Bump. No idea how to do this ? Am i the only one to work daily on Nucleo while targeting a not-that-easy-to-use board ? :p
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.