cancel
Showing results for 
Search instead for 
Did you mean: 

Code generation issue with Discovery board B-L072Z-LRWAN1

NicRoberts
Senior II

I have a Discovery board B-L072Z-LRWAN1 and I am trying to set up a project using CubeIDE but get the following,

NicRoberts_0-1768308697317.png

So I check to see if the L0 & LRWAN packages are in the repository,

NicRoberts_1-1768308848946.png

Yes, they're there. I click OK & Cube carries on setting itself up & up pops the ioc window. I press configure & generate & get some C code but the build option is greyed out.

 

What am I missing here?

 

 

 

10 REPLIES 10

Thanks Mattias, I was confused about why it wasn't finding the FW in the repository as this wasn't an issue with any of the other boards we use.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.