2022-05-09 4:40 AM
My code generation fails with the following exception :
Exception in thread "Thread-4645" java.lang.IllegalAccessError: class parsers.FromScratchParser (in unnamed module @0x6a84a97d) cannot access class com.sun.org.apache.xerces.internal.parsers.DOMParser (in module java.xml) because module java.xml does not export com.sun.org.apache.xerces.internal.parsers to unnamed module @0x6a84a97d
at parsers.FromScratchParser.getDestinations(FromScratchParser.java:257)
at convertor.Convertor.generate(Convertor.java:354)
at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.generate(ToolchainGenerator.java:370)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:4150)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:916)
at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:54)Here's my java version
�?� java --version
openjdk 18.0.1.1 2022-04-22
OpenJDK Runtime Environment (build 18.0.1.1+2)
OpenJDK 64-Bit Server VM (build 18.0.1.1+2, mixed mode)Full log is attached.
Solved! Go to Solution.
2022-06-15 9:00 AM
I had the exact same issue. The issue is that STM32CubeMX does not support java 18, only java 11.
On Arch, STM32CubeMX can be configured to use java 11 on a per-application basis by editing /usr/bin/stm32cubemx (or creating in a location in $PATH with precedence) to use an explicit runtime, for example:
#!/bin/sh
exec /usr/lib/jvm/java-11-openjdk/bin/java -jar /opt/stm32cubemx/STM32CubeMX "$@"or on a system-wide basis by running `archlinux-java set java-11-openjdk`
2022-06-15 9:00 AM
I had the exact same issue. The issue is that STM32CubeMX does not support java 18, only java 11.
On Arch, STM32CubeMX can be configured to use java 11 on a per-application basis by editing /usr/bin/stm32cubemx (or creating in a location in $PATH with precedence) to use an explicit runtime, for example:
#!/bin/sh
exec /usr/lib/jvm/java-11-openjdk/bin/java -jar /opt/stm32cubemx/STM32CubeMX "$@"or on a system-wide basis by running `archlinux-java set java-11-openjdk`
2022-06-15 9:18 AM
Amazing, thanks for the explantation !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.