2025-07-15 6:13 AM - last edited on 2025-07-15 6:19 AM by Andrew Neil
Recently, The CubeMX cannot open IOC files through the file menu, and cannot save IOC files when creating a new project. But I can open the project normally by double clicking an existing IOC file.
Working environment: Win11+CubeMX6.15
I have tried reinstalling CubeMX, lowering CubeMX version to 6.13, and so on, but they all have the same problem.
Solved! Go to Solution.
2025-07-15 6:44 PM
Today, after multiple restarts of the computer, all functions surprisingly returned to normal.
2025-07-15 6:42 AM
Hello @YouXiaoquan
Could you please add your IOC file in order to investigate the issue?
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-15 6:49 AM
2025-07-15 7:22 AM
Hello @YouXiaoquan
I am not able to reproduce the issue; I can use the Load Project successfully.
Could you start CubeMX using command line and check if there are any errors?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-15 7:38 AM
This issue is not related to the specific IOC file. Specifically, when using the "Load Project" and "Save Project" menus, CubeMX did not respond.
2025-07-15 6:44 PM
Today, after multiple restarts of the computer, all functions surprisingly returned to normal.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.