2023-04-11 1:59 AM
I get an error when trying to open .ioc file of the project. It was working fine and i am pretty sure I haven't changed anything about it. Just can't open it anymore for some reason. Also the name that it says that is the right one, is the same as the name of my file.
The error I get:
Invalid Input: Must be project's active .ioc file.
Project's 'camera_module' active one is 'camera_module.ioc' file
2023-04-11 3:30 AM
Hello @PPopo.1
First let me thank you for posting .
Here are a few steps you can try to resolve this issue:
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.