2023-09-23 8:03 PM
I have stm32 bluepilll on which I am able to transmit CAN messages but CAN Receive interrupt is not generating.
I found while configuring that CAN RX pin(GPIO mode) is getting configured as Input mode. How accurate is this?
I think it should be Alternate function. I made PB8 as Alternate function still CAN Rx interrupt is not working.
Above statements are under stm32f1xx_hal_msp.c
I am using CAN RX1 interrupt, following are my configurations
static void MX_CAN_Init(void)
{
/* USER CODE BEGIN CAN_Init 0 */
/* USER CODE END CAN_Init 0 */
/* USER CODE BEGIN CAN_Init 1 */
/* USER CODE END CAN_Init 1 */
hcan.Instance = CAN1;
hcan.Init.Prescaler = 9;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_3TQ;
hcan.Init.TimeSeg2 = CAN_BS2_4TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = ENABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = ENABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN_Init 2 */
CAN_FilterTypeDef canfilterconfig;
canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
canfilterconfig.FilterBank = 18; // which filter bank to use from the assigned ones PA11
canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO1;
canfilterconfig.FilterIdHigh = 0x00000103<<5;
canfilterconfig.FilterIdLow = 0;
canfilterconfig.FilterMaskIdHigh = 0x00000103<<5;
canfilterconfig.FilterMaskIdLow = 0x0000;
canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
canfilterconfig.SlaveStartFilterBank = 20; // how many filters to assign to the CAN1 (master can)
HAL_CAN_ConfigFilter(&hcan, &canfilterconfig);
if (HAL_CAN_Start(&hcan)!= HAL_OK)
{
Error_Handler();
}
HAL_CAN_ActivateNotification(&hcan,CAN_IT_RX_FIFO1_MSG_PENDING);
/* USER CODE END CAN_Init 2 */
}
void HAL_CAN_RxFifo1MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO1, &RxHeader, RxData);
if (RxHeader.StdId == 0x0000103)
{
rx=1;
}
}
2023-09-24 6:06 AM
__weak void HAL_CAN_RxFifo0FullCallback(CAN_HandleTypeDef *hcan)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(hcan);
/* NOTE : This function Should not be modified, when the callback is needed,
the HAL_CAN_RxFifo0FullCallback could be implemented in the user
file
*/
}
Why can't you use this function for receive message? I generated the project using your micro part number.
2023-10-16 2:07 AM
Hello, i have the same configuration Suryaprakash2002. CAN RX does not trigger also for me. I do not know what to do. CAN TX transmit well, CAN RX does not trigger. The scope shows the recieved CAN at the CAN_RX PA8 PIN. What i noticed is that after a can message received the CAN TX pin PA9 goes for some bits(2 or 3) low and then high again.
Any ideas?
Best regards
2023-10-17 5:39 AM
CAN RX1 interrupt it does not work. You do not have to change the filters.
I found an alternative solution for not triggering the interrupt:
At CubeMX go at Connectivity->CAN->Configuration->NVIC->
-USB low priority or CAN RX0 interrupt (activate)
-CAN RX1 interrupt (deactivate)
Then the CAN communications works well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.