2017-03-13 7:52 AM
1. Faulty code generation
STMCube Generates to following code in the function: void SystemClock_Config(void)
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;�?
this results that the SystemClock_Config function always enters the Error_Handler
HSE Clock is used as main clock.
By removing the RCC_OSCILATORTYPE_HSI define code functions normally2. Non working code USB MSC
Code generated for USB MSC stops working after the usb command USB Set Configuration Request
Device Manager reports Error Code 10 (can't start device)
The usb analyzer tool of wireshark shows no communication after host sends Set Configuration Request.
Problem observed from at least STM32CubeMX V4.18+
Changing driver versions does not solve the isuue
Tested on STM32446e-Eval and STM23F446ZC
PC: Windows 10 Toolchain: KEIL µVsion V5 #stm32cube-bug #bug-stm32cubemxSolved! Go to Solution.
2017-04-28 12:24 AM
Hello all,
Sorry for our late answer.
I would inform you that this issue is fixed in
V 4.20.1.Sorry for any inconvenience this may cause you.
BR. Eric
2017-03-13 8:09 AM
Hi
Zwarteveld.Johan
,Thank you for your feedback. The issue has been reported to our MX team for check..Sorry for the inconvenience it may bring.
-Nesrine-
2017-03-17 5:03 AM
For future reference :
2. Non working code USB MSC
Code generated for USB MSC stops working after the usb command USB Set Configuration Request
Device Manager reports Error Code 10 (can't start device)
The usb analyzer tool of wireshark shows no communication after host sends Set Configuration Request.
Problem observed from at least STM32CubeMX V4.18+
STM32CubeMx generates:
USBD_StatusTypeDef USBD_LL_Init (USBD_HandleTypeDef *pdev)
{
/* Init USB_IP */
if (pdev->id == DEVICE_FS) {
/* Link The driver to the stack */
hpcd_USB_OTG_FS.pData = pdev;
pdev->pData = &hpcd_USB_OTG_FS;
hpcd_USB_OTG_FS.Instance = USB_OTG_FS;
hpcd_USB_OTG_FS.Init.dev_endpoints = 6;
hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL;
hpcd_USB_OTG_FS.Init.dma_enable = DISABLE;
hpcd_USB_OTG_FS.Init.ep0_mps = DEP0CTL_MPS_64;
hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED;
hpcd_USB_OTG_FS.Init.Sof_enable = DISABLE;
hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE;
hpcd_USB_OTG_FS.Init.lpm_enable = DISABLE;
hpcd_USB_OTG_FS.Init.vbus_sensing_enable = ENABLE;
hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE;
if (HAL_PCD_Init(&hpcd_USB_OTG_FS) != HAL_OK)
{
Error_Handler();
}
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_FS, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 0, 0x40);
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_FS, 1, 0x80);
}
return USBD_OK;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
if the following line is changed from:
hpcd_USB_OTG_FS.Init.dev_endpoints = 6;�?�?
to
hpcd_USB_OTG_FS.Init.dev_endpoints = 4;�?�?
the code start working again and my OS recognizes the device as mass storage.
is suspect that the set configuration command fails because there are an additional 2 uninitialized / unused endpoints
Please include the mentioned abnormalities in the next update
2017-03-17 11:21 AM
THANK YOU for posting this. Spent like 3 days measuring everything electrically trying to figure out why an HSE was not being selected. This bug is the reason, now works like a charm.
2017-03-30 5:53 AM
Thanks a lot, change 4 boards, 2 IDEs
µVsion and SW4STM32, HSE still not work, Now running good.
2017-04-28 12:24 AM
Hello all,
Sorry for our late answer.
I would inform you that this issue is fixed in
V 4.20.1.Sorry for any inconvenience this may cause you.
BR. Eric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.