2018-02-14 7:53 PM
STM32CubeMX Version: 4.24.0
Target MCU: STM32F103RFTx LQFP64
Target IDE: Atollic TrueStudio
Steps to reproduce:
first
time, it successfully generates the codesecond
time, an error occurs:'The Code is successfully generated under C:/ProjectX/Firmware/MainBoard
but TrueSTUDIOproject generation have a problem'The tail of the log file shows the exception:
...
2018-02-15 14:43:53,475 [INFO] CodeEngine:179 - oldGeneratedFile, C:\ProjectX\Firmware\MainBoard\Src\main.c_save2018-02-15 14:43:53,690 [INFO] CodeEngine:197 - Generated code: C:\ProjectX\Firmware\MainBoard\Src\main.c2018-02-15 14:43:53,902 [INFO] ProjectBuilder:1243 - Time for Copy HAL[2] : 8mS.2018-02-15 14:43:53,913 [INFO] ProjectBuilder:1711 - Project Generator version: 2.27.02018-02-15 14:43:53,925 [INFO] ConfigFileManager:448 - The Die is : DIE4302018-02-15 14:43:56,164 [INFO] ToolchainGenerator:124 - stack trace : java.lang.NullPointerException at generators.TrueStudioGenerator.setFiles(TrueStudioGenerator.java:1228) at convertor.Convertor.generateTSTKProject(Convertor.java:1230) at convertor.Convertor.generateTrueStudioFiles(Convertor.java:1113) at convertor.Convertor.generate(Convertor.java:653) at convertor.Convertor.convert(Convertor.java:559) at convertor.Convertor.updateProject(Convertor.java:412) at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.update(ToolchainGenerator.java:118) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:1769) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:594) at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)2018-02-15 14:43:56,165 [INFO] ToolchainGenerator:125 - [Project Generator] Problem in the update of the project2018-02-15 14:43:56,166 [INFO] ConfigFileManager:741 - mx.scratch is deleted!2018-02-15 14:43:56,166 [INFO] ProjectBuilder:1777 - Time for Generating toolchain IDE Files: 2260mS.2018-02-15 14:43:56,166 [ERROR] ProjectBuilder:1783 - Error in Project Generation2018-02-15 14:43:56,166 [ERROR] ProjectBuilder:610 - Error in Project GenerationThis failure is consistent and repeatable. It is also severe as it is stopping progress on this project.
If I revert the project to the last known good state, I can rerun the steps above.
Please let me know if you need any further details to resolve this urgent issue.
Thanks -
:: Gavin
#code-generation #truestudio #bug #cubemx2018-02-14 9:20 PM
Some additional information which may be relevant: the project in question has been converted to have a C/C++ Nature.
2018-02-24 3:37 AM
Hi, I have the same problem...
It occurs on both C and C++ projects, no differenceI tried on several PCs but nothing has changed
The problem emerged with the latest version of
STM32CubeMX 4.24
The previous one worked fine
Thanks
Rodolfo
2018-02-26 4:23 AM
Hello,
Please share your ioc file to check this issue.
Best Regards,
Imen
2018-02-26 6:55 AM
Hello Imen,
Thank you for your interest, and please excuse my bad english.
I enclose two examples and the sequence for replicating two different problems that emerged in the latest release of CubeMX.
Example N.1
You can open the working project 'Reel-Working' with TrueSTUDIO, you will see that you can rebuild it without problems. If you regenerate the project with CubeMX, you should get this error (image: Project generation error.PNG).Now, if you rebuild it, you should see the file 'system_stm32l0xx.c' duplicated in two folders (image: Build error.PNG).
Example N.2
Starting from the Mxt.ioc file, you generate the project. You should see, by opening it with TrueSTUDIO, that it is not possible to compile it. Although there are files related to CMSIS and RTOS, from project explorer are not visible, it is probably just a problem of paths, I have not investigated the problem because at the moment I'm working on something else.I've been working with TrueSTUDIO for about 2 years, I'm not an expert, but I've never had this problem before.
I found the same problem on other projects too, it is very repeatable.
If you need more precise information, do not hesitate to ask.Thank you!
Best Regards
Rodolfo
________________ Attachments : Project generation error.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxw4&d=%2Fa%2F0X0000000b2U%2FFQRZ5OGBY7eZrioGGMbeQ7wa.l5qmhDW7OTdqbPG.xA&asPdf=falseMxt.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxvM&d=%2Fa%2F0X0000000b2R%2FePiEDr9QJNweyarC2hyi0JDAOJwU_VDKX.2FrC61qtQ&asPdf=falseReel-Working.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxwE&d=%2Fa%2F0X0000000b2W%2Fxh9msODhQJYMgwIlOv7VafA5TDMrfiuUNZgrk8S2wGs&asPdf=falseBuild error.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxbg&d=%2Fa%2F0X0000000b2T%2FeQeL8CLdFTttfHXJ8q71w6f7uaiRU22Z34NXI69KZ2c&asPdf=false2018-03-01 6:55 PM
I have a similar problem. All I wanted to do was create a F4Discovery project with FreeRTOS, once FreeRTOS was enabled, I could not get the project to be generated correctly. No change in settings other than the checkbox.
________________ Attachments : FirstTrueStudioF4Disco.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxvf&d=%2Fa%2F0X0000000b2N%2F9Z6wcW6dGIA.X_aEfNf.JGZ17NQNdLHhOpvV3Wg7QnQ&asPdf=false2018-03-05 5:57 AM
Hi
gavin.baker
,Beck.Joseph
,Vigilante.Rodolfo
,This issue will be fixed in the next CubeMX release (4.25).
Please upgrade your CubeMX release as soon as it is available.
BR. Jeanne
2018-11-15 8:59 AM
I still see this problem with CubeMX V4.27.0.
It worked fine at beginning. But after I modified code in TrurStudio, it start to get problem.
Please help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.