2025-10-27 9:36 PM - edited 2025-10-27 9:46 PM
When I try and enable UART5 in the .n657_dk2.ioc file, the development system seems to go into an infinite loop with the mouse cursor spinning endlessly.
Bug1: To replicate,
1- open the n657_dk2.ioc file
2- goto the connectivity section
3- enable UART5 in FSBL
4- change mode to Asynchronous
5- set Hardware Flow control to RTS/CTS.
system hangs....
Bug 2: if you try and save the file, it corrupts the file and you cannot edit the .ioc file anymore.
.ioc file attached
IMPORTANT!!! I need a fast work around so I can go to layout this week....
2025-10-28 12:39 AM - edited 2025-10-28 2:45 AM
Hello @matt-crc
After following your scenario to replicate the issue, I found that the problem described above and in the other thread is the same, but appears under two different scenarios. Both scenarios have been escalated to the development team for further investigation (internal ticket number 220572 ).
CubeMX hangs , and if you then try to save the .ioc file, it becomes corrupted because CubeMX is no longer functioning correctly. Therefore, I believe your scenario is invalid, and the main issue is the underlying problem that caused CubeMX to crash in the first place
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-28 4:36 PM
Hello @Ghofrane GSOURI
Regarding Bug2: you should consider this a real serious bug. Corrupting user files is a REAL BIG issue, regardless whether the CubeMX task has stopped functioning. You really need to implement some sort of safety mechanism instead of wiping out user files. Please escalate.
Note: it takes a lot of time to re-enter all the data.... ask me how I know.
Can you also acknowledge BUG 3 where the clock pins cannot be allocated properly and creates a bunch of errors when attempting to do this. This was brought up in another post (which you were mentioned/tagged in).
thanks
Matt
2025-10-29 1:10 AM
Hello @matt-crc
Thank you for your feedback. I agree that corrupting user files is a serious issue. Even if we add safety mechanisms, they may not always work if CubeMX crashes or hangs unexpectedly. In such cases, there is still a risk that user files could be affected.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.