2025-07-26 6:23 AM
Missing pre-processor symbol check in file "Middlewares/ST/ST_Cryptolib/Inc/Commonn/types.h"
current line 49:
#if !defined(_STDINT_H) && !defined(__stdint_h) && !defined(_STDINT) new line 49:
#if !defined(_STDINT_H) && !defined(__stdint_h) && !defined(_STDINT) && !defined(_GCC_STDINT_H)To solve this bug add ``&& !defined(_GCC_STDINT_H)`` on line 49.
Cheers,
Andreas
2025-07-28 12:37 AM
Hello @hga3
First let me thank you for posting.
I would appreciated if you could share your IOC or at least provide more details about the MCU .
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-30 1:53 PM
Hi Ghofrane
Thank you for looking into this. I am using GCC (13.2.1 20231009) on GNU/Linux. The details about the MCU and some relevant CubeMX and FW versions are listed below.
Please ask if you need more information to reproduce it. I receive a compile error without patching the mentioned file. I use the following patch -- see attached file, to solve the issue after a fresh creation or update via CubeMX.
Best wishes,
Andreas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.