STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

How to install ARM CMSIS.* packages

Posted on June 28, 2018 at 15:32How can I installed ARM.CMSIS.*.*.pack into STM32CubeMX software components?  I was able to include the package into STM32CubeMX 'Embedded Software Packages Manager', but it won't installed.The errors were missing CMS...

Resolved! Upgrading STM32Cube MX plugin in Atollic

Posted on July 06, 2018 at 13:47I use Rowley (personal favorite), IAR and Atollic depending on the customer's requirements.  I have a project which I am trying to work on now in Atollic.  I have in Atollic the STM32CubeMX perspective version 4.25.  ...

STM32H7x3 - Ethernet Desc Allocation in D2 SRAM

Posted on April 17, 2018 at 13:13Hi All,I am working on Ethernet in STM32H7 and I am unable to understand two things :1) What is the need to avoid memory allocation of ETH_Tx and ETH_Rx Desc  in D1 SRAM ?I have seen an example in 'STM32Cube/Reposito...

STM32F107vct6 cubemx+ RMII+DP83848+LWIP

Posted on July 11, 2018 at 07:31HelloI want config STM32F107vct6 in cubemx to use RMII+DP83848+LWIP without oscilator(I connect PA1 and PA8 to X1)but in STM32CubeMX->Configuration->ETH->External PHY configuration->PHY is  LAN8742A_PHY_ADDRESS and ca...

0690X0000060MERQA2.png 0690X0000060MEWQA2.png 0690X0000060M6hQAE.png 0690X0000060M6mQAE.png
h_kabiri by Associate II
  • 1380 Views
  • 1 replies
  • 1 kudos

USB composite device CDC+HID

Posted on April 19, 2018 at 18:11Hi,i have working HID example with me. But i was trying to integrate CDC class in the existing HID class. I am using cubemx code. After initializing and flashing i got the error as 'Device Descriptor Request Failed' ...

SS.Sagar by Associate III
  • 10194 Views
  • 15 replies
  • 0 kudos

The best way to convert non-CubeMX project to STM32CubeMX ?

Posted on July 10, 2018 at 19:25Hello, can somebody share the most efficient steps to convert non-MX project to a STM32CubeMX structured one? Most (or all?) of the Cube examples are not MX-generated hence they are not structured accordingly. So far ...

eBirdman by Senior II
  • 3230 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.