STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

what are the necessary configurations needed for can protocol

i had intialized can1 and can2 of my stm board but after writtingthe whole code only transmission of messages is happening on both the boards but not the receiving.but when iused one board for transmission and one for reception its working properly.s...

AGaja by Associate II
  • 2261 Views
  • 4 replies
  • 0 kudos

I can't seem to get STM32CubeMX to start.

It gives a dialog that says some path is missing in the registry or the JRE is corrupt. I tried removing and reinstalling JRE, then reinstalled CubeMX. Nothing seems to help. There were some entries in the registry under JavaSoft. Seems like CubeMX n...

RBlac by Associate
  • 614 Views
  • 0 replies
  • 0 kudos

How to include codes from examples

Hi,I am using Nucloe144 H743 board, Cube Mx and true studio. I want to incorporate codes given in cubeH7 example for EVal boads. How i can do this? For example how i can use FatFs application Code for EVAL boards in Nucleo or Other Custom boards......

Resolved! STM32CubeMX 5.0.1 No vertical bar for window scrolling

The vertical scroll bar in the GPIO Settings window used in various peripheral does not appear.Left-click on a timer (for example), in the central window you can see the "Configuration -> Parameter Settings" with the vertical scrol bar, this is OK. I...

0690X000006D8q7QAC.jpg 0690X000006D8qCQAS.jpg

How to configure PHY in MII mode using cubeMX?

I want to work on ethernet using MII mode. At times i am getting struck in clock configuration also. In lwip.c file, the link is getting up but while pinging the board from pc am getting destination host unreachable. Please help to resolve the proble...

PSrin by Associate
  • 2010 Views
  • 3 replies
  • 0 kudos

CubeMX: How to DELETE configuration of a peripheral?

Suppose you configure a timer, then decide you don't want that one.How is one supposed to remove it?I've tried delete key, all views, finally edited the IOC file.Really now! This user interface would get us canned if we delivered it to a customer...T...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.