STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

hello world with ADC crashes on STM32F051

Hello,I ran into a problem with a STM32F051K6T and cannot figure out where the problem is.With Cube I configure the controller with UART (TX-only 115.2kBd) and polling on ADC_IN0.The generated code for uVision compiles and loads errorfree.But even th...

Manitux by Associate
  • 1213 Views
  • 2 replies
  • 0 kudos

ADC input voltage range in differential mode

In STM32CubeMx H7(v1.5.0) the example of ADC_DifferentialMode for NUCLEO-H743ZI is showing that we can measure difference voltage range of 6V6 in this mode and readme,txt file is also clearly telling us that we can vary the input voltage from -3V3 to...

0690X000009Z2xqQAC.png

Found a bug with the latest rev of STM32CubeMX Rev 5.3.0

I just migrated to CubeMX Rev 5.3.0. I'm developing a project for the Nucleo STM32F429ZI board. My target toolchain is Keil MDK-ARM V5. I'm using mostly the LL function libraries. I'm using the latest FW_F4 V1.24.1 package. Bug: As soon as regenerate...

MSilv by Associate
  • 834 Views
  • 0 replies
  • 0 kudos

SensorTile and CubeMX integration

Hello, I've been learning and using CubeMX a lot for project generation. I work with VS code and compile via make through the generated makefile and it is going pretty good.Now I have to work with the SensorTile and I really wish to use the cube con...

ANist by Associate III
  • 2921 Views
  • 6 replies
  • 0 kudos

Unable to install patch 1.10.1 for STM32F0 offline

I tried to install the en.patch_cubefw_f0.zip package from the "From Local ..." menu in the "Embedded Software Packages Manager" and I receive the message "Missing dependency for this package. - STM32Cube FW_F0 V1.10.0". Unfortunately, the "missing" ...

HAL_TIM_PeriodElapsedCallBack Doesn't works.

Hello,I upgraded cube on version 1.5.3 and function HAL_TIM_PeriodElapsedCallBack stopped working.I found out that program never goes trough function HAL_TIM_PeriodElapsedCallBack .I think that the problem is in initialization , because you need to ...

0690X000009Z8GoQAK.png 0690X000009Z8GjQAK.png 0690X000009Z8GZQA0.png 0690X000009Z8GeQAK.png
NIvez by Associate
  • 1270 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.