STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

STM32H747 Hardware Semaphore Interrupt

EDIT: Nevermind this thread can be deleted, apologies. I didn't enable the HSEM2 Global interrupts under NVIC1/2 in CubeMX.Hi,I'm having issues getting the hardware semaphore interrupts to function correctly, or I'm misunderstanding their usage. I'm ...

savvn001 by Associate II
  • 1813 Views
  • 1 replies
  • 0 kudos

Building file systems/projects with STM32CubeMX

Hello, I bought the STEVAL-IDP003V1D evaluation board and I want to create a "custom" IO-Link slave device that, I can hook up to an existing IO-Link Master. Then write commands from the master and receive a response from my slave. I found the IO-Lin...

Soepoe by Associate II
  • 879 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F4xx USB bug, when compiled by GCC using -O3 option.

Setup:Project, generated by CubeMX and compiled by arm-none-eabi-gcc-9.2.0 toolchain. CubeMX firmware package version: STM32Cube FW_L4 V1.14.0CPU: STM32L432KCY (and others)Toolchain: arm-none-eabi-gcc-9.2.0 (and others)Compiler options: -mcpu=cortex...

0690X00000AtA3eQAF.jpg 0690X00000AtA4cQAF.jpg

Resolved! STM32H7 RMII timing

Hello,We are using STM32H743ZIT6 revision V.This is connected to an ethernet PHY device via RMII. The PHY outputs the 50MHz RMII REFCLK to drive the RMII on the STM.According to the following sources, the RMII TX data lines (TXD0 and TXD1) should be ...

0690X00000BumlfQAB.png 0690X00000BumluQAB.png
graffiti by Associate III
  • 4889 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.