STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! LL_TIM_*() calls take too much time.

I am having a problem with a timer. I use CubeMX LL drivers, with basic time-base timer configuration.STM32L100RCT6, TIM6 and TIM7. Core Clock = 32MHz, PCLK1 (TIM6 and TIM7) = 32MHzPrescaller = 31, which should set timer to tick at 1us. ARR value is ...

0690X00000BvalaQAB.png

Generated code doesn't call HAL_NVIC_SetPriorityGrouping

BUG REPORT:Using STM32CubeIDE 1.1.0 with a new STM32F401VE project, under the CubeMX perspective, when I change the system core priority grouping, it correctly limits the range of values that I can enter for the interrupt pre-emption priority and sub...

Tom V by Associate
  • 1793 Views
  • 2 replies
  • 0 kudos

Resolved! hello community of STM, I want to perform a simple lwip ethernet ping test using the raw api without RTOS on STM32H743ZI2 Nucleo Board but so far I haven't met with any success. Can I please be provided with some support?

I have used stm32cubeMX and atollic truestudio in this case. I'm attaching my project folder which contains the ioc file and the code files. I would be highly obliged if anyone can tell me the mistakes in either the cubeMX settings or the code or bot...

MMish.1 by Associate II
  • 7285 Views
  • 4 replies
  • 0 kudos

STM32CubeMX 5.4.0 released

Dear communityWe are pleased to announce the release of STM32CubeMX v5.4.0What is new in STM32CubeMX V5.4.0? • Added the support of the STM32L5 Series (beta support)(a): – Possibility to create projects with no TrustZone® security (user Option Byte T...

Resolved! [SOLVED] STM32F4 USB works intermittently

I'm using an STM32F411RET6 MCU to make a keyboard. Attached is the full schematic. Using CubeMX to generate the USB code. I'm a hobby-ist and I apologize in advance if there's a very basic issue that I've overlooked.The problem is it works sometimes ...

0690X00000BvWGOQA3.png
Zang Man by Associate III
  • 2796 Views
  • 4 replies
  • 0 kudos

Resolved! Exclude files from update in cubemx

Hi! I changed usb hid.c file not in user code. After I change something in cubemx and regenerate code this file is also changed to its oryginal form. ​Is there a way to tell cubemx not to change this specyfic file?​

oeliks by Senior
  • 1767 Views
  • 3 replies
  • 0 kudos

NUCLEO-F767ZI UART3 TX DMA NOT WORKING

I've created a new project just to send a string over UART3 TX via DMA. The non-DMA version workes fine...so I'm not sure what I'm doing wrong here. I think I had configured the cube correctly...so I'm stuck. Can someone help me take a look at the...

AAoe.1 by Associate II
  • 1177 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.