STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1762 Views
  • 0 replies
  • 2 kudos

STM32CUbe MX db files usability in an external tool(s)

I started small project, where I use "db/plugins/clock" XML file(s) from CubeMX to visualize the state of the clock-tree in the running STM32.Currently I face number of issues. Mybee you can direct me to other resources more suitable than CubeMX file...

UART4 Unavailable on STM32F750N8-DK?

I want to use only the Tx pin on UART4, it is on PA0/CN5-1 of the Arduino connector. I setup// Initialize UART4 for Debug Terminal 250 kbaud using 50 MHz PCLK1 /////////////////////////////////   PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHC...

DRobe.4 by Senior
  • 1579 Views
  • 3 replies
  • 0 kudos

Resolved! stm32h7 dtcm ram overflowed

Hello, I am relatively new in this field, and need assistance for my project at work.Recently, in order to have more RAM, I switched from STM32F4 to STM32H7. I saw that STM32H7 has 1MB of RAM, and decided to base our system on this MCU. However, afte...

VYoun by Associate III
  • 8052 Views
  • 13 replies
  • 0 kudos

Resolved! about RTC calibration! by use for LSI clk. (STM32F091V)

I use STM32F091VI use LSI for RTC clock.I know that LSI is inaccurate.I set the RTC interrupt to 1 second.However, the interrupt interval was 860ms.Can anyone tell me how to calibrate the RTC?I am happy with the sample source code.

Ukazu by Associate III
  • 2143 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.