STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX code not working with USB

Hello!I have project created with CubeMX. I coded a lot there and then I wanted to add a USB CDC device with CubeMX. After code generation I compiled the project and I got an error message:../Inc/usb_device.h:61:22: fatal error: usbd_def.h: No such f...

Resolved! CubeMX - search for alternative pins does not work

In CubeMX version 6.20, board Nucleo-H743ZI2: I want to find alternatives for SPI1_MOSI. Default is PD7 but all examples use PA7.So I ctrl/click on PD7 and expect that CubeMX will show me PA7. But it does not.Well maybe it finds it, but does not show...

Pavel A. by Super User
  • 1787 Views
  • 5 replies
  • 0 kudos

How to compile and run in a single command? Keil Bug?

All I want to do is make a change to the code and then compile and run on the target without the debugger, ideally with a simple keyboard shortcut.Simple example using the ST NUCLEO-F030R8 board and a Keil project auto-generated using ST's STM32CubeM...

martincho by Associate II
  • 1132 Views
  • 0 replies
  • 0 kudos

When I have the MX program set up CAN1 on my STM32F446 Nucleo-64 the generated code fails to initialize with the default values from MX.

it generates the following init using the default parameters:static void MX_CAN1_Init(void) {   /* USER CODE BEGIN CAN1_Init 0 */   /* USER CODE END CAN1_Init 0 */   /* USER CODE BEGIN CAN1_Init 1 */   /* USER CODE END CAN1_Init 1 */ hcan1....

KiptonM by Lead
  • 2100 Views
  • 3 replies
  • 0 kudos

Resolved! STM32Cubemx and datasheet pin description mismatch!

Hello, I am an engineer working at Desird Arge Design. I had a problem with the STM32G031F6P6 processor. I think there is an error while selecting the timer channels in the STM32 Cubemx application. According to the datasheet description, TIM1; It in...

SDura.2 by Associate
  • 1777 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.