STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

How to enable a slave timer but not triggering it.

I`m hoping to have a slave timer enabled but idling and wait to be triggered by a master. The idea is to have the slave to trigger ADC reading for multiple cycles and synchronized with the master:My timer config are shown belowWhen I call functions s...

0693W00000NrMIjQAN.jpg 0693W00000NrMJ8QAN.jpg
Zef.M by Associate
  • 1673 Views
  • 1 replies
  • 0 kudos

Where is the rank N°1 settings? (ADC / STM32L151RETx)

I try to set, using last version STM32CubeIDE, the ADC to get 8 analog inputs, using DMA, with permanent conversion.I doesn't see anymore the rank 1 ? (see picture)When I start HAL_ADC_Start_DMA, i have only the AN0 value, and only 8 bits (I set12bit...

0693W00000NqKIzQAN.jpg
lclor by Associate III
  • 3557 Views
  • 5 replies
  • 0 kudos

[Cube OTG USB] [Minor issue]incorrectly @param description on HAL_StatusTypeDef USB_FlushTxFifo(USB_OTG_GlobalTypeDef *USBx, uint32_t num)

The original param description: * @param num FIFO number *    This parameter can be a value from 1 to 15      15 means Flush all Tx FIFOsAccording to stm32h7 reference manual, it should be: * @param num FIFO number *    This parameter can be a value ...

Resolved! How to change chip selection after a project is created

Hello, I'm programming using STM32H753. But I realized that the chip I chose when I was creating the project was STM32H743. Is there any way to change the chip settings in a project that has already been created? Should we re-create a new project unc...

Ekim.1 by Associate II
  • 4714 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.