STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Why can't I download firmware package?

Hello. When I tried to use Motor Control Bench for the first time in a while, I had trouble downloading the firmware package.Looking at the log file at the time of code generation, the code appears to be generated.Do you know if the generated code is...

0693W00000QL2LCQA1.png

STM32CubeMX not working on Win11 for ARM in emulated mode

I've tried to run STM32CubeMX on my Windows 11 parallels virtual machine that run under Monterey on Apple M1 MAX machine.For some reasons the application crash. I've tried various compatibility modes with and without administrative rights but with no...

ABucs by Associate II
  • 1832 Views
  • 2 replies
  • 0 kudos

Resolved! UBEMX generated EXTI IRQ handler with wrong symbolC

I have two gpios enabled one as an output another as a interrupt input. PA11 and PI11 respectively. There are two pin defines generated by CUBEMX, for argument call them MYPINA_Pin and MYPINB_Pin respectively. For the interrupt handler CUBE generates...

FColl.1 by Associate III
  • 2340 Views
  • 5 replies
  • 1 kudos

Resolved! How do I add FreeRTOS threads without CubeMX deleting them?

I created a project for an STM32H753 MCU and have added FreeRTOS via CubeMX called from CubeIDE. CubeMX generates the following code in main.c: /* Init scheduler */ osKernelInitialize(); /* Call init function for freertos objects (in freertos.c) */ ...

RLein.1 by Associate III
  • 3768 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeMx 6.6.1 show wrong FDCAN Parameters Setting

The latest version of STM32CubeMx 6.6.1 organizes the parameters of the FDCAN differently from the previous version and shows useful information on Time Quantum, Time for one Bit and Baud Rate.But I think the displayed parameters are wrong, as shown ...

ALomb.1 by Associate III
  • 1688 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.