STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

IRRemote on STM32L4RI-DISCO

Hi, I'm new to STM32. I have an STM32L4RI-DISCO board and would like to add an IR receiver and decode RC5 signals. According to AN4834, IRTIM can be used on STM32L4. I have downloaded en.x-cube-irremote.zip.Firstly it is not recognized by Cube MX.Sec...

Lanceh by Associate III
  • 2193 Views
  • 3 replies
  • 0 kudos

Resolved! STPackCreator Global/Project define.

Hi all.Working with the Pack Creator I know I can create a header file that contains defines that are editable in the CubeMX view.I'd like to know if it's possible to have a pack that places defines in the project settings instead of a header file? 

pywtk by Associate II
  • 2059 Views
  • 3 replies
  • 0 kudos

STPackCreator with H5 Discovery Kit

Hi all!I'm creating a pack using the Pack Creator. My pack uses a BSP template. I've tried creating projects using the pack for a selection of boards. In all cases bar the H5 the pack template successfully creates the right #include for the platform ...

pywtk by Associate II
  • 1038 Views
  • 0 replies
  • 1 kudos

Twice used Pin Lables in CubeMX

Hello,because of my mistake, I had assigned the same label for two different pins within CubeMX 6.12. It seems, CubeMX recognize this, but send not an error oder a warning message about it. What happen, CubeMX is attaching the port- and pinname to th...

JPiet.3 by Associate III
  • 1671 Views
  • 1 replies
  • 1 kudos

Resolved! Flash memory - STM32F030C8 Erase Cycles

Hello I'm using STM32F030C8.I'm writing the code because I want to use the internal flash memory like rom.Is there a set number of times I can write in internal flash memory? If there is a related document, I would like to see it.Thank you.

giwonKIM by Associate III
  • 2250 Views
  • 5 replies
  • 3 kudos

Resolved! the Pinout and Configuration .ioc is wrong

I have been using STM32F767zi for long time.I know some of the pin feature by heart.Last night, I enabled ETH for a moment and to see what pin it uses, then I disable it and then all the chaos happened.I realized that many of frequently used USART 2,...

Wai Siang by Associate III
  • 4036 Views
  • 2 replies
  • 1 kudos

Resolved! Why is I2S Frequency in Clock Configuration so high?

Hi STM community!I am new to STM microcontrollers and this is my first post :)My board is a tiny STM42F401CCU6 @ 84MHz. I already have made some first steps with CubeMX and CubeIDE, after I came from the arduino IDE which was a bit too simple (readin...

Stipe_0-1721847172491.png
Stipe by Associate II
  • 2842 Views
  • 1 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.