2020-02-11 5:34 AM
Hi there,
I am using the latest CubeMX to generate code for B-L475-IOT01A with FREERTOS and X-CUBE-BLE1 4.4.0. However the code it generate does not even build. I tried various samples, including SensorDemoBLESensor, Beacon, but yield the same result.
The build message indicated that MX_BlueNRG_MS_Init() is missing. Apparently it is missing an entire suite of source code. I attempt to port the code over from a Nucleo sample code but was unsuccessful.
Please kindly help to fix. Thanks!
2020-02-11 9:02 AM
Yeah I've complained about the same issue over a year ago with support. I too can't get it to compile without so many errors. I still haven't seen ST fix the compile errors since then.
2023-03-22 7:24 AM
Any answer?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.