2021-02-03 12:35 AM
Hello ,
I'm using the latest STM32Cube with NUCLEO144-H743ZI2 board.
I am a complete beginner with using the STM32 and STM32Cube. I came from the ESP32 world, where everything was relatively easy. Through numerous attempts, I can now handle the STM32Cube (especially the STM32CubeMX), even if some terms that appear there are still unknown to me.
At the beginning I set the goal to get the TSL2591 sensor running. Communication with this component takes place via the I2C bus (I2C1).
In the STM32CubeMX I have specified that the pins PB8 and PB9 should be used for SCL and SDA respectively. In the generated code I cannot see this definition anywhere! That is my first problem.
When I debug the code, calling the procedure "tsl2591_initialize()" leads to calling the function "I2C_IsAcknowledgeFailed()" in the file "stm32h7xx_hal_i2c.c", lines 6377ff. The first query of the flag "I2C_FLAG_AF" says that this flag is set. The execution of the following loop "while (__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_STOPF) == RESET)" is exited, but the code afterwards leads to the return with error. I can't recognize the reason for this. Probably something is missing in my code.
What am I doing wrong?
Can anybody help me to get this code running?
I've put the entire project in the attachment.
Thanks in Advance,
Michael
2021-02-03 12:46 AM
Hi @Mick P. F.
I'll answer you on the first question linked to CubeMX and configuration pins.
In fact, the code of GPIO Configuration is generated under stm32xxx_hal_msp.c file, you can find there all pins configured for each IP used.
Hope this information helped you, Khouloud
2021-02-03 12:52 AM
Hello Khouloud,
Many thanks for your tip!
Now I know where to find the initialization/configuration code, but that doesn't help me to solve the runtime problem.
2021-02-03 1:14 AM
It looks like the device doesn't answer your request on the bus. The HAL API requests that "The device 7 bits address value in datasheet must be shifted to the left before calling the interface", see HAL_I2C_Mem_Read description.
2021-02-03 2:18 AM
Hello KnarfB,
That was my (first) mistake... I've seen this before, but I didn't think anything of it.
Many thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.