2024-10-21 11:31 AM
Hi,
I got some problem with using ADC Differential Mode.
When I am using ADC Single Ended Mode:
Channel 8 Reading: ~8735
Channel 9 Reading: ~10907
When I am using ADC Differential Mode:
Reading: ~7106
That's weird. ADC Differential Mode should be subtracting both reading so suppose I should get 8735-10907=-2172? Why I will get 7106? Is it the signing problem? I already use int16_t instead of uint16_t
Does anyone can help me on this?
Thank you!!!!
Solved! Go to Solution.
2024-10-21 12:15 PM - edited 2024-10-21 12:16 PM
Differential conversion results are mid-centered and half-gain to fit the full range.
8192 + (-2172 / 2) = 7106.
See relevant sections of ADC chapter in RM.
JW
P.S. Read also relevant sections of datasheet, note the rather limited common-mode range.
2024-10-21 12:15 PM - edited 2024-10-21 12:16 PM
Differential conversion results are mid-centered and half-gain to fit the full range.
8192 + (-2172 / 2) = 7106.
See relevant sections of ADC chapter in RM.
JW
P.S. Read also relevant sections of datasheet, note the rather limited common-mode range.
2024-10-21 12:19 PM
Hi,
Oh I see! Thank you so much!!!!
2024-10-21 12:28 PM
Hi,
But is there anyway to directly output signed value from ADC?
2024-10-21 4:56 PM
Try data alignment "right adjust"
2024-10-21 11:05 PM
> But is there anyway to directly output signed value from ADC?
See Offset section of Data management subchapter of ADC chapter in RM, and description of ADC_OFRy register.
JW
2024-10-22 7:46 AM
Hi,
Thank you so much! I did it!
ADC1->OFR1 = 0; // Clear the offset register first
ADC1->OFR1 |= (8192 << ADC_OFR1_OFFSET1_Pos); // Set the OFFSET to 8192
ADC1->OFR1 |= (1 << ADC_OFR1_SSAT_Pos); // Enable signed saturation
ADC1->OFR1 &= ~(1 << 24); // Set POSOFF to 0 (negative offset)
ADC1->OFR1 |= (8 << ADC_OFR1_OFFSET1_CH_Pos); // Apply the offset to ADC Channel 1
And also set left shift bit by 1 to mutiply the result by 2.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.