2024-10-14 3:55 AM
Hello,
Would it be possible to have the correspondence of the JSON type according to the type of variable we put? Please
I've been able to identify a few such as :
type 1 -> uint8_t
type 3 -> uint32_t
Best regards
Solved! Go to Solution.
2024-10-14 4:34 AM
Hello
The information is available in the description of the "write panel" node. It is :
In order to help other users, if this is answering your question, please mark it as answered. Thank you.
2024-10-14 4:34 AM
Hello
The information is available in the description of the "write panel" node. It is :
In order to help other users, if this is answering your question, please mark it as answered. Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.