2020-03-08 5:58 AM
In the hardware requirements for the STM32CubeMonitor it is mentioned that an “STM32 target board“ is required. (wiki)
Does that mean that the monitor is not compatible with J-Link and J-Link OB and for example an STM32L433CC ?
Solved! Go to Solution.
2020-03-09 10:43 AM
Hello
J-Link and J-Link OB are not supported by STM32CubeMonitor. Version 1.0.0 supports only ST-Link probes (or boards including ST-Link like Nucleo).
Best regards
Stephane
2020-03-09 10:43 AM
Hello
J-Link and J-Link OB are not supported by STM32CubeMonitor. Version 1.0.0 supports only ST-Link probes (or boards including ST-Link like Nucleo).
Best regards
Stephane
2020-05-27 3:30 PM
Any plans to support J-Link in the future?
2020-05-28 12:10 AM
Hello
There is no plan to support this probes right now.
Best regards
Stephane
2020-12-22 2:18 AM
That's such a pity. J-Link is such a popular probe and having to switch between an ST-Link and J-Link to use this application is just extra hassle. Could you not contact Segger and ask for assistance in adding support?
2021-04-02 1:32 AM
Up
2021-04-04 12:02 PM
Up from my side also..
2021-11-30 11:56 PM
2022-03-08 7:03 AM
Upvote
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.