2025-11-11 8:29 AM
Hello,
I am trying to use STM32Cube Monitor USB PD with custom board.
I see ST link v3 minie on a trace port. but I can't see any traces at all. Is there a dedicated package in CubeMX i can enable to see USB-PD traces ? Thank you.
Solved! Go to Solution.
2025-11-13 10:45 PM
Hi grisom13
I confirm USART1 should work with STM32CubeMonitor UCPD.
For further help please share your ioc.
-------------------
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-11 8:55 AM - edited 2025-11-11 5:05 PM
Ok, looks like the Trace enable in under Utilities section
UPD. Added code by Cube MX. I see the USART1 rate changed to 921600 from 115200 in Main.C but still the Trace screen is empty.
I am following the below article:
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Source
1 - I am using USART1 115200, not LPUART - is this OK ?
2- Do i need to unable GUI for USBPD monitor ?
2025-11-12 6:17 PM
No Advise ? :(
2025-11-13 7:10 AM
2025-11-13 9:48 AM
Hello,
I have STM32G0B1KBU3N MCU. Currently my Custom PCB has only USART1. RX and TX pins connected to ST Link V3 minie. Please confirm this can work with USB-PD STM32 monitor.
2025-11-13 10:45 PM
Hi grisom13
I confirm USART1 should work with STM32CubeMonitor UCPD.
For further help please share your ioc.
-------------------
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.