2025-09-20 3:16 AM
Iam using cube monitor which is off course a very useful tool for debugging but only difficulty iam facing is when i disable the variables which i don't want to see or completely invisible, could you please bring in something so that it can be visible even if disabled. Ex image below
If you see above image the disabled variables are completely invisible for me to make them enable again.
2025-09-25 8:32 AM
Hello @STuser2
You would like to have an option to hide/unhide variables from the graph upon clicking on their name, is that right?
2025-09-25 9:58 AM
What i am trying to say is that even if i make variables as hidden, after some time i may want to watch the variables (hidden) again so it should be partially visible instead of completely hidden.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.