2020-04-29 12:18 AM
I tried to get the variable "g_counter1" in 80 micro-seconds for the STM-Studio Example project using CubeMX_ver.5.6.0 and EWARM_ver.8.42.1.
But the result was not as good as the attachment below.
-STM32_CubeMonitor_Result_dashboard_g_counter1.PNG
-Log_myVariables_2020-04-29_14h35m16s.zip
(Log_myVariables_2020-04-29_14h35m16s.stcm)
In the first place, can CubeMonitor be obtained in 80 microseconds?
In addition,
MCU: STM32G0431KB(NUCLEO-G431KB)
This setting information is the following attached file.
-STM32_CubeMonitor_Setup1_Block_diagram.PNG
-STM32_CubeMonitor_Setup2_Variable_AquisitionParameters.PNG
-STM32_CubeMonitor_Setup3_Probe_Protocol_Frequency.PNG
The setting value of this source code is the following attached file.
-STM32_CubeMonitor_SourceCode1_dataAqc.c.PNG
-STM32_CubeMonitor_SourceCode2_dataAqc.h.PNG
Thank you for your guidance.
Solved! Go to Solution.
2020-04-29 1:10 AM
Hello
I think it is not possible to monitor continuously the counter every 80 micro seconds.
In snapshot mode, STM32CubeMonitor tool will retrieve the data by buffer : The value are stored in the target in a circular buffer, and STM32CubeMonitor collects the data in buffer as fast as possible. We knows that it takes more than 1ms to read one u32 data, so reading the snapshot buffer will take few ms. (Need to read data and header). So the data buffer is likely to overflow.
This could explain the strange curve you have attached, I see a repeated pattern with :
So I don't think that 80 microsecond is reachable. You should try with slower speed, it should give better results.
Best regards
Stephane
2020-04-29 1:10 AM
Hello
I think it is not possible to monitor continuously the counter every 80 micro seconds.
In snapshot mode, STM32CubeMonitor tool will retrieve the data by buffer : The value are stored in the target in a circular buffer, and STM32CubeMonitor collects the data in buffer as fast as possible. We knows that it takes more than 1ms to read one u32 data, so reading the snapshot buffer will take few ms. (Need to read data and header). So the data buffer is likely to overflow.
This could explain the strange curve you have attached, I see a repeated pattern with :
So I don't think that 80 microsecond is reachable. You should try with slower speed, it should give better results.
Best regards
Stephane
2020-04-29 3:38 PM
HI,Stephane,
Thank you for your reply immediately.
I understand well.
Best regards,
RIG
2020-04-29 3:39 PM
HI,Stephane,
Thank you for your reply immediately.
I understand well.
Best regards,
RIG
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.