2023-12-08 10:25 AM
Hai:
I am using STMcube IDE 1.13.2 and TouchGFX 4.22.1 in my project. Once flash the program to the traget, If i given play but program not run. Once i press the RESET button or Power ON and OFF then it will work.
This happend only in 1.13.2 IDE version.
What i do for this issuse? Kindly help me for this issuse.
Thanks & Regards
Govind M
2023-12-08 10:37 AM
Debug it, see where execution is at. The cpu is likely doing something.
You can attach the debugger without flashing/resetting if you modify the debug configuration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.