2019-06-19 12:34 AM
I also have the STLink-V3 which I can't use with the STLink GDB in SWD mode because the only speed available is 24000KHz and fails downloading code. Using the probe with OpenOCD leaves me with no SVW support. In STM32CubeProgrammer the SWD speed is selectable???
Good to have Segger support.
When are this STM32 tools fully supported?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.