2023-07-19 4:41 AM - edited 2023-07-19 4:44 AM
I don't know if this is new but it sprang into my eyes today when I started STM32CubeIDE after a couble of days of pausing. It's Version 1.13.0 now.
I was about to create a New project in the project tree view and the configurator page popped up.
In the left corner appears - and I didn't notice this before - a yellow alert message, saying
/!\ STM32 target or STM32Cube example selection is required
I didn't choose anything at this point int time, so why such an ugly warning? Is something missing? Peculiar: my workspace has been migrated and still is workspace_1.4.0.
2023-07-19 6:03 AM - edited 2023-07-19 6:37 AM
Hello chriskuku,
it's just a message to say that you have to select a device or an example, without you cannot continue.
BR
2023-10-25 11:25 AM
I stil (Version 1.13.1 STM32CubeIDE
Version: 1.13.1
Build: 17479_20230728_0839 (UTC)
OS: Linux, v.6.1.0-13-amd64, x86_64 / gtk 3.24.38
Java vendor: Eclipse Adoptium
Java runtime version: 17.0.6+10
Java version: 17.0.6), when I try to create a new project. I saw this Problem as well on 1.13.2.
2023-10-25 11:26 AM
.... I stll have this Problem
2023-10-25 11:36 AM
When I start a new Project, it chechs the database and then immedialety
2023-10-26 12:05 AM
Hi Badi,
Can you try to explain step by step your way to create a project ?
For ex:
- Login with my st.com account (don't forget to check the connection (window->preferences->STM32CubeIDE->Firmware Updater -> check connection button)
- File -> New -> STM32 Project
- in the MCUs/MPUs List, choose a device, for ex STM32F401...
- Next
- Field the project name
- Finish
HTH
2023-10-26 9:17 AM
2023-11-05 7:33 AM
I'm having the same problem. Any solutions?
2023-11-05 7:51 AM
I have found this solution, maybe helps for you
https://community.st.com/t5/stm32cubeide-mcus/target-selection-stm32-target-or-stm32cube-example-selection-is/m-p/598007#M21299
2023-11-05 7:58 AM
read old post...
For ex:
- Login with my st.com account (don't forget to check the connection (window->preferences->STM32CubeIDE->Firmware Updater -> check connection button)
- File -> New -> STM32 Project
- in the MCUs/MPUs List, choose a device, for ex STM32F401...
- Next
- Field the project name
- Finish
++ so FIRST select a cpu...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.