2024-05-27 9:17 AM - edited 2024-05-27 9:33 AM
I'm currently testing Tracealyzer but I'm having problems in using it in streaming mode. I followed the indications in video "Visual trace diagnostics with STLINK-V3, Percepio Tracealyzer and DevAlert" (https://www.youtube.com/watch?v=rZlSuq7TySA) to setup ITM but it seems not to be working. SWV is enabled, clock is set as on target, "Shared ST_LINK" flag seems to have no effect, ITM Stimuls Port is set correclty.
- Tracealyzer 4.8
- STM32CubeIDE 1.15.1
- ST-Link V3 or ST-Link V3 Mini (same result)
- No RTOS (bare metal)
- Custom board
Once the system is set up according to the video, if I start debugging from STM32CubeIDE, starting tracing from Tracealyzer gives the error "Unable to select and reset device" (in the Tracealyzer setting window the ST-LinkID is recognized correclty). The SWV Trace Log window in STM32CubeIDE shows the activity.
If I start the trace from Tracealyzer I can't start debugging from STM32CubeIDE as it stops at the ST-Link firmware verification with the error "No ST-LINK detected".
Seems like it's not possible to access the ST-Link at the same time from the two systems.
Snapshot tracing is working instead.
Do someone has the same issue? How can it be solved?
Solved! Go to Solution.
2024-05-27 9:58 AM
>Seems like it's not possible to access the ST-Link at the same time from the two systems.
Right, try to have two drivers in one car - same problem . :)
So use IDE/debug , OR Tracealyzer/whatever this is.
2024-05-27 9:58 AM
>Seems like it's not possible to access the ST-Link at the same time from the two systems.
Right, try to have two drivers in one car - same problem . :)
So use IDE/debug , OR Tracealyzer/whatever this is.
2024-05-28 1:07 AM
Hi @AScha.3 , thank you for your reply.
You're definitely right, watching the video more carefully I realized they show exclusive use, debugger or analyzer. :eyes:
Working as expected. :thumbs_up:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.