2024-01-03 12:59 PM
As others before me, I wish to make my own serial number in a USB CDC device. This isn't the problem – I know how to do that.
However, I am puzzled about how the unique serial number is generated in the code auto-generated in STM32CubeIDE. Specifically the functions Get_SerialNum() and IntToUnicode() in usbd_desc.c.
/**
* @brief Create the serial number string descriptor
* @PAram None
* @retval None
*/
static void Get_SerialNum(void)
{
uint32_t deviceserial0;
uint32_t deviceserial1;
uint32_t deviceserial2;
deviceserial0 = *(uint32_t *) DEVICE_ID1;
deviceserial1 = *(uint32_t *) DEVICE_ID2;
deviceserial2 = *(uint32_t *) DEVICE_ID3;
deviceserial0 += deviceserial2;
if (deviceserial0 != 0)
{
IntToUnicode(deviceserial0, &USBD_StringSerial[2], 8);
IntToUnicode(deviceserial1, &USBD_StringSerial[18], 4);
}
}
/**
* @brief Convert Hex 32Bits value into char
* @PAram value: value to convert
* @PAram pbuf: pointer to the buffer
* @PAram len: buffer length
* @retval None
*/
static void IntToUnicode(uint32_t value, uint8_t * pbuf, uint8_t len)
{
uint8_t idx = 0;
for (idx = 0; idx < len; idx++)
{
if (((value >> 28)) < 0xA)
{
pbuf[2 * idx] = (value >> 28) + '0';
}
else
{
pbuf[2 * idx] = (value >> 28) + 'A' - 10;
}
value = value << 4;
pbuf[2 * idx + 1] = 0;
}
}The three 32-bit values retrieved in lines 12 - 14 above, are together the Unique device ID of the microcontroller (UID[95:0]. For me, it would make sense to use all 96 bits or 24 hex digits to generate a unique ID. As the descriptor is supposed to be written the UTF-16, this would be a string of 48 bytes. I have read elsewhere, that the maximum number of bytes for any descriptor is 126 + 2 bytes. Yet, the constant USB_SIZ_STRING_SERIAL constant in usbd_desc.h limits the descriptor to 24 + 2 bytes, i.e. 12 UTF-16 characters.
To "fit" the 24 hex digits into half the size, the code "shrinks" the UID by adding UID[31:0] and UID[95:64] together, for the first 8 digits, and then uses half of UID[63:32] for the remaining 4.
Can anyone explain why? Am I missing something? Can the serial number really only be 12 hex digits in length?
2024-01-03 1:11 PM - edited 2024-01-03 1:12 PM
It was an implementation decision to have serial numbers of that length, not a USB requirement/restriction. Serial numbers can be longer but become unwieldy at some point.
The odds of a serial number conflict with 12 hex digits are quite small (1:281 trillion).
2024-01-03 1:13 PM - edited 2024-01-03 1:13 PM
It can be longer than 12 characters. Maybe some old host systems have problems with longer strings.
2024-01-03 1:40 PM
> The odds of a serial number conflict with 12 hex digits are quite small (1:281 trillion).
That would hold if they would be random. They are not.
OTOH, the examples are just that, examples. Nobody really cares.
JW
2024-01-03 3:17 PM
Okay, thanks a lot gentlemen. I appreciate it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.