2025-03-23 7:04 PM
I cannot figure out how the USB sets the Function selector output.
URB Function: URB_FUNCTION_GET_DESCRIPTOR_FROM_DEVICE (0x000b)
URB Function: URB_FUNCTION_SELECT_CONFIGURATION (0x0000)
URB Function: URB_FUNCTION_SELECT_INTERFACE (0x0001)
I can modify bRequestType and bRequest, but that does not affect the URB Function selected just after the IRP ID and IRP USBD_STATS info.
eg. Wireshark Dump:-
0b 00 is URB Function: URB_FUNCTION_GET_DESCRIPTOR_FROM_DEVICE (0x000b)
When I select configuration, the 0b 00 becomes 00 00, but how? I cannot find any place in the firmware or hardware, that relates to this?
Am I making sense?
2025-03-23 7:09 PM
Beginning at 80 06 05 03 above is the FIFO out, so where does the preceeding bytes come from?
2025-03-23 11:11 PM
I am thinking that winpcap creates this term and number (URB_FUNCTION_GET_DESCRIPTOR_FROM_DEVICE (0x000b)) and that it is not an actual number directly sent over USB?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.