2021-06-13 5:52 PM
I closed out of my project last night, and tried opening it today and kept having it just freeze on the homepage of the STM32cubeide. I even tried creating a new project and nothing. I even tried reinstalling but still same error. When I try to close out of the program, it won't let me either. I have to use task manager. The error message I get when I do try and close it is "Could not initialize class java.awt.Toolkit." Thank you for any help.
2021-06-14 4:15 AM
First are you able to work without any issue if initating a new workspace location ?
If no I would advice you to unsinstall and reinstall back your STM32CubeIDE tool.
If yes get a try to remove .metadata/.plugins/org.eclipse.e4.workbench/workbench.xmi from your workspace (see https://stackoverflow.com/questions/2481089/where-does-eclipse-save-the-list-of-files-to-open-on-startup).
You may face an issue opening back an editor from a previous session having ended such session not in a normal way (kill, crash, ...) leading to unstable state at restart.
2021-12-11 6:59 AM
The same problem I am facing but follow the above steps but still the problem not resolve. And I am trying last from a few days to create stm32 file searching everywhere but stilll I am not able to solve the problems please help me to get out of this.thank for your any help
2021-12-11 8:30 AM
I followed the same steps which are given by cartu38 OpenDev. First I tried by changing the workspace then I uninstalled and reinstalled it again. And also removed metadata/.plugins/org.eclipse.e4.workbench/workbench.XML file from the workspace. But still, I am not able to create the stm32 project. This first time I have such worst experience with any IDE. Please help if any one know about this. I have been trying this problem since a week and it is very important to resolve this error.Please help me .Again I am requesting please help me.
2021-12-11 9:35 AM
How you hope that anyone helps you without providing any details?
Please give away some details: Windows or Linux? If Linux, which one? Has the IDE worked ever on your machine before or this is the 1st time?
If you have Windows, try to re-install it to clean state.
2021-12-11 8:40 PM
Sorry, I have not provided os details. My stm32cube IDE is running on the windows os. Earlier I worked a total of 30 days on this application. Now when I am working on this application this does not allow me to create an stm32 project. when I am trying to close this application this is giving me the error "Could not initialize class java.awt.Toolkit. ".I tried with a new workspace and also I do reinstall this application. And deleted workbench.xmi this file also. But still, the problem is not resolved. Is there anything that I am missing? Please somebody help me. please..please ...very urgent. Thanks in advance.
2021-12-11 9:23 PM
@Pavel A. As you said what is re-install it to clean state. This is different then normal install state.
2021-12-13 4:59 AM
Hi @AMISH.2 Thank you for the info.
Such problems are often fixed by creating a new workspace. But it did not work for you so...
Windows is a complex and open system, there's a lot of things that can break.
If getting productive fast is important to you, do a complete re-install of Windows. Ask your IT person to help.
2022-01-09 4:41 AM
Use another IDE!!! like KEIL IAR or anyother. STMCUBEIDE is not a profissional tool.
2022-04-25 2:39 PM
Same issue. However, this software worked fine before my fresh installation of windows.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.