2023-03-16 11:01 PM
Hi all, im a beginner on stm32 (currently using l703rz) to play with. I have tried the code from stm32 stepbystep (Intro to UART), the build and debugging are a success. The problem is that it keeps shutting down after debugging and would not send out "HelloWorld" to my teraterm. The ports connected are same (115200 and 8 bits).
Anyways, here are the code that i newly tried
uint8_t Test[] = "Hello World !!!\r\n"; //Data to send
HAL_UART_Transmit(&huart2,Test,sizeof(Test),10);// Sending in normal mode
HAL_Delay(1000);
Below here is the output after i tested these lines of code above.
STMicroelectronics ST-LINK GDB server. Version 7.1.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
Log output file: C:\Users\Alpha\AppData\Local\Temp\STM32CubeProgrammer_a07796.log
ST-LINK SN : 066AFF353638425043085244
ST-LINK FW : V2J40M27
Board : NUCLEO-L073RZ
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x447
Revision ID : Rev Z
Device name : STM32L07x/L08x/L010
Flash size : 192 KBytes
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0x41
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a07796.srec
File : ST-LINK_GDB_server_a07796.srec
Size : 10.43 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 83]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.346
Verifying ...
Download verified successfully
Shutting down...
Exit.
2023-03-17 12:46 AM
Ok so the programming of the code to the board seems to complete.
if you press the reset button does your code run then?
Are you starting in the debugger?
2023-03-22 9:14 AM
Good day,sir. I have noticed and found out that it was a very very simple mistake that should not be made when referring to stepbystep guide as i missed the most important part. The problem had been solved and the shutting down command invokes is for the ide itself. I once again apologize for my silly mistake.
Btw,sir, is there any place where i can learn the gpio and adc function? I am currently trying to get voltage reading from ph sensor (ph4502c) into my l073rz, but the voltage reading keeps going higher than usual. For example, if I use arduino uno,I can get the pH sets at 2.5v (ph7) and can even adjusts the pot 1 near bmc connector while in stm32 l073rz i seem to not able to do so when the reading is higher than its supposed to and the value is not stable at all. The connection of pH sensor goes like this
Ph sensor nucleol073rz
V+ = 5v
Gnd = gnd
Po = pa1 (pin)
2023-03-23 2:43 AM
The sensor PH-4502C is supplied with 5V and also outputs voltages up to 5V, which you cannot measure directly with a 3.3V supplied STM32. To convert its larger voltage range to the range for STM32, you need a matching circuit, in the simplest case a voltage divider or one with an opamp as a voltage follower.
In addition, the reference voltage of the NUCLEO-L073RZ is connected to VDD (which can vary), so you always measure ratiometrically. For an absolute value measurement you have to:
Hope it helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.