2022-06-22 2:25 PM
If i try to use this BSP of the above version and integrate with project generated from Cube IDE then many issues happen. for example problems with STM32H747_Discovery_Camera.
Also integrating the touch controller with touchgfx is not working and instead of providing ideas here maybe you try it by your self on some discovery boards and show us or simply back to the older BSP Version.
2022-06-25 7:25 AM
You mix two not relevant thinks. FW_H7 and BSP. Try show code part and what dont work instead for example ...
2022-06-25 7:39 AM
The underlying problem here is that the code is often not well tested, and the H747I-DISCO doesn't have the camera mounted, so it's a random variable, so support is unlikely to be broad.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.