2024-04-30 12:54 AM
Hello! I sorley need some help integrating my tensorflow.lite model on the STM32F405RGT6, which i have on a custom board. I have converted the model to a Carray.h but I am struggeling to include the tensorflow lite micro library. I would appreciate a step by step tutorial on how to include it and how to make it work. I am using this bib: https://github.com/tensorflow/tflite-micro and I can not get it to work using this guide: https://community.st.com/t5/stm32-mcus/how-to-add-external-libraries-in-stm32cubeide/ta-p/628619#:~:text=After%20creating%20a%20project%20for,%3E%20MCU%20GCC%20Linker%20%3E%20Libraries. I am struggeling with this step in particular i think: "Now that the external library is linked to the project, the header file can be included by doing the following: Navigate to Project -> Properties -> C/C++ Build -> Settings -> Tool Settings -> MCU GCC Compiler. Include paths, and then add the path to the header file." If anyone has any knowlegde or experince using tf lite micro on STM32 I would appreciate tips and tricks as well! Thank you so much beforehand!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.