2023-12-15 1:49 AM
Hi.
I have recently encountered a problem that I'm not capable of solving in for a few hours now.
I'm using STM32F042K6T6 as a uC and, when I try to debug my projet, it shows me the following errors:
Failed to execute MI command:
target remote localhost:2331
Error message from debugger back end:
Remote communication error. Target disconnected.: No error.
Failed to execute MI command:
target remote localhost:2331
I'm trying to fix those problems for a few hours, but with no succes.
Can someone help me solve me this?
Also I'm using J-LINK as a debugger.
Best regards
2023-12-15 2:39 AM
Hello @ItzNicolo and welcome to the community,
Could you, please, provide the debug configuration and the GDB server log? This will help us to analyze the problem further. Also, check that the J-Link is correctly connected to the board. This knowledge base link may help.
Thanks,
Rim
2023-12-15 3:52 AM
Ok, here is my debug configuration:
For GDB Connection Settings:
1. Autostart local GDB server
2. Host name or IP address: localhost
3: port number: 2331
My Debug Probe is SEGGER J-LINK
For GDB Server Command Line Options:
1. Interface: SWD
2. Initial Speed: 4 MHz without specific J-LINK S/N
3. Device: STM32F042K6T6
4. Reset strategy: Type 0: Normal
5. JTAG Scan Chain: Auto with no position and IRPre
For Serial Wire Viewer:
1. Core Clock is disabled
2. Limit SWO clock is disabled
3. RTOS Kernel Awareness is disabled
For Misc
1. No script file used
2. Live expressions and Flash download verification are enabled
2025-01-16 1:46 PM
What ended up being the solution for this error message?
2025-01-17 5:06 AM
I don't know. I just restarted the app and the error message disappeared.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.