2019-08-09 10:23 PM
When trying to generate code using STMCubeMX, both TrueStudio (understandable) and STM32CubeMXIde are greyed out. I have the newest version of CubeMX, CubeMXIde, and TrueStudio installed.
When will the 757 be supported? We are in a rush in developing a major prototype project (we have been waiting for DSI support forever on the H7 line) and now that it's available, support for it is far from complete. There seems to be no mention of it being supported or not anywhere.
Thoughts? The 753 is supported, so why not the 757? There aren't very many differences between the two parts (except for DSI and the power supply).
Solved! Go to Solution.
2024-09-02 6:27 AM
Hello,
This an old thread but, STM32CubeMx, STM32CubeIDE (deprecated TrueStudio) and STM32CubeProgrammer support STM32H7 dual core years ago including STM32H757 devices.
2024-09-02 6:27 AM
Hello,
This an old thread but, STM32CubeMx, STM32CubeIDE (deprecated TrueStudio) and STM32CubeProgrammer support STM32H7 dual core years ago including STM32H757 devices.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.