2022-02-15 10:25 PM
I have a project (https://github.com/carlk3/Digital-Automotive-Generator-Voltage-Regulator) that I've been developing in STM32CubeIDE on (Ubuntu) Linux. Now I want to move it to STM32CubeIDE on Windows. I'm using GitHub for source code management (SCM), and also, eventually, to share the project. I've tried a few different ways to clone the project from GitHub to Windows, but I haven't been able to come up with a buildable project in STM32CubeIDE. Most recently, I installed and set up EGit (Git integration for Eclipse), and was able to use it to Import the project, but it won't build. I get 3185 errors, 73 warnings. Here is a sample:
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os.h:240:20: error: expected declaration specifiers or '...' before 'osThreadId_t'
240 | #define osThreadId osThreadId_t
| ^~~~~~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os.h:510:24: note: in expansion of macro 'osThreadId'
510 | int32_t osSignalClear (osThreadId thread_id, int32_t signals);
| ^~~~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os2.c:1791:109: error: expected '=', ',', ';', 'asm' or '__attribute__' before '{' token
1791 | osStatus_t osMessageQueueGet (osMessageQueueId_t mq_id, void *msg_ptr, uint8_t *msg_prio, uint32_t timeout) {
| ^
../Middlewares/Third_Party/FreeRTOS/Source/include/event_groups.h:742:60: warning: type defaults to 'int' in declaration of 'uint32_t' [-Wimplicit-int]
742 | void vEventGroupSetBitsCallback( void *pvEventGroup, const uint32_t ulBitsToSet ) PRIVILEGED_FUNCTION;
| ^~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os.h:510:46: error: unknown type name 'int32_t'
510 | int32_t osSignalClear (osThreadId thread_id, int32_t signals);
| ^~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os.h:510:46: error: unknown type name 'int32_t'
510 | int32_t osSignalClear (osThreadId thread_id, int32_t signals);
| ^~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/include/queue.h:1385:79: error: unknown type name 'BaseType_t'
1385 | BaseType_t xQueueReceiveFromISR( QueueHandle_t xQueue, void * const pvBuffer, BaseType_t * const pxHigherPriorityTaskWoken ) PRIVILEGED_FUNCTION;
| ^~~~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/include/event_groups.h:742:69: error: expected ';', ',' or ')' before 'ulBitsToSet'
742 | void vEventGroupSetBitsCallback( void *pvEventGroup, const uint32_t ulBitsToSet ) PRIVILEGED_FUNCTION;
| ^~~~~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/include/event_groups.h:743:62: warning: type defaults to 'int' in declaration of 'uint32_t' [-Wimplicit-int]
743 | void vEventGroupClearBitsCallback( void *pvEventGroup, const uint32_t ulBitsToClear ) PRIVILEGED_FUNCTION;
| ^~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os.h:516:11: error: expected declaration specifiers before 'osEvent'
516 | os_InRegs osEvent osSignalWait (int32_t signals, uint32_t millisec);
| ^~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os.h:516:11: error: expected declaration specifiers before 'osEvent'
516 | os_InRegs osEvent osSignalWait (int32_t signals, uint32_t millisec);
| ^~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os2.c:1832:63: error: expected '=', ',', ';', 'asm' or '__attribute__' before '{' token
1832 | uint32_t osMessageQueueGetCapacity (osMessageQueueId_t mq_id) {
| ^
../Middlewares/Third_Party/FreeRTOS/Source/include/queue.h:1391:1: error: unknown type name 'BaseType_t'
1391 | BaseType_t xQueueIsQueueEmptyFromISR( const QueueHandle_t xQueue ) PRIVILEGED_FUNCTION;
| ^~~~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/include/event_groups.h:743:71: error: expected ';', ',' or ')' before 'ulBitsToClear'
743 | void vEventGroupClearBitsCallback( void *pvEventGroup, const uint32_t ulBitsToClear ) PRIVILEGED_FUNCTION;
| ^~~~~~~~~~~~~
../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os.h:247:19: error: expected declaration specifiers before 'osTimerId_t'
247 | #define osTimerId osTimerId_t
| ^~~~~~~~~~~What am I missing?
Solved! Go to Solution.
2022-11-18 9:20 AM
Thanks, Simon.
I found the problem, which was that I used the "Generate peripheral initialization as a pair of .c/.h files per peripheral", so a file named "freertos.c" was generated. In order to export various queue, timer, mutex, and event handles from that file I had created a file name "freertos.h". On Windows, which isn't so picky about case sensitivity, this conflicts with "Middlewares\Third_Party\FreeRTOS\Source\include\FreeRTOS.h".
2022-10-28 6:01 AM
Hi,
I came across your ticket by chance.
If you have not solve your problem: this can simply be a problem between linux and windows about "LF" and "CRLF" newline.
Maybe you can use a linux to windows file converter. Or maybe there is something done inside Git to make it works correctly.
Regards,
Simon
2022-11-18 9:20 AM
Thanks, Simon.
I found the problem, which was that I used the "Generate peripheral initialization as a pair of .c/.h files per peripheral", so a file named "freertos.c" was generated. In order to export various queue, timer, mutex, and event handles from that file I had created a file name "freertos.h". On Windows, which isn't so picky about case sensitivity, this conflicts with "Middlewares\Third_Party\FreeRTOS\Source\include\FreeRTOS.h".
2022-11-21 1:10 AM
Glad to hear you found the solution and thanks for sharing.
You should mark your reply as the Answer ;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.