2024-11-06 11:05 PM
I just try using Nucleo L522ZE-Q and compile example code
after i debug it, somehow it cannot write the file to the flash
and the trace is not set properly
after i downgrade the IDE using 1.14 it can work properly no
please fix the new IDE, i didn't want to use multiple version of cube IDE
Thanks
Solved! Go to Solution.
2024-11-06 11:14 PM
Hello @Azwar and welcome to the ST Community.
Are you having the same limitation number 189229 on the https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.16.x#STM32L5
And if so, can the workaround mentionned with the debug issue "Use OpenOCD as a debug probe" solve your issue.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-06 11:14 PM
Hello @Azwar and welcome to the ST Community.
Are you having the same limitation number 189229 on the https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.16.x#STM32L5
And if so, can the workaround mentionned with the debug issue "Use OpenOCD as a debug probe" solve your issue.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-07 12:23 AM
Yes, it work now
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.