2024-09-04 12:52 AM - edited 2024-09-04 1:36 AM
Hello everyone,
I want to make a usb connection using USB_OTG_FS_DP and USB_OTG_FS_DM pins on the STM32U575 board. When I tried it with the examples found on the internet, it didn't work. When I tried the same method on the STM32F401 board, it was enough to select only USB_OTG_FS -> Device Only and Middleware -> USB_DEVICE -> virtual com port. What basic settings do I need to make to see my STM32U575 board as a virtual com port on the computer? I'm not very experienced in this. Thank you in advance for your help. Also, when I use the ux_device_cdc_acm example in CubeIDE, it does not appear as a virtual com port.
2024-09-04 2:39 AM - edited 2024-09-04 2:39 AM
Hello @beenwew ,
Ensure that the correct driver is installed and verify that the heap and stack sizes are sufficient.
Did you try the USB CDC example within STM32U5 firmware?
2024-09-04 3:09 AM - edited 2024-09-04 3:12 AM
Yes, I tried the ux_device_cdc_acm example for the nucleo u575zi in the cube ide application. All I did was debug and plug in the usb type c cable and upload this example to the card.
2024-09-13 2:09 AM
When I used the ready code of CubeIDE, I managed to run it with only a typec cable, but I want to connect with DP and DM pins without typec. For this, I created a project without USBPD. In this case, the PC does not see the device on the NUCLEO board, but on the PCB board I designed, it sees it as an unknown device. DFU mode works fine on my PCB.
When I debug the code, it goes into an infinite loop in the
/* Wait here for the PendSV to take place. */
__tx_wait_here:
B __tx_wait_here // Wait for the PendSV to happen
section of the tx_thread_schedule library.
2025-09-03 8:37 AM
I use AZRTOS with USBX on stm32L562 for composite USB and i have this same problem - @beenwew do you resolve problem ? debug stay in this same place on:
B __tx_wait_here // Wait for the PendSV to happen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.