2025-02-11 3:37 AM - edited 2025-05-22 4:52 AM
Hello all,
I'm working with the STM32N6-Discovery board on a camera application. I'm finding every so often when launching the debugger it will get a "Target not responding" error. Sometimes days go by where I can't debug my code until it randomly starts working again. Power cycling and restarting CubeIDE doesn't help. I know it isn't my code as the ST video encoder examples also give me the same error despite working fine the day before. I've also tried adding a breakpoint on the reset vector to see if it was a system init problem, however the error occurs before the code starts running.
IDE - CubeIDE 1.18.1
Board - STM32N6570-DK
I'm wondering if it's a memory or library issue as when I temporarily remove all camera and encoder related code from my project, it runs fine.
[6.593] WaitConnection(): Accepted connection on port 61234...
[6.593] WaitConnection(): Waiting for connection on port 61234...
[6.594] run(): GDB session thread running
[6.594] handleSessionEvent(): GdbSessionManager, session started: 2
[6.594] Device_GetStatus(): ST-LINK device status: Failed to get status, Target not responding, retrying... 32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.