2025-10-27 3:22 AM - last edited on 2025-10-27 3:38 AM by Andrew Neil
Hi, im using stm32h745bit6 MCU, when im pressing reset button only M7 core is reseting and M4 core is stucking in an reset handler itself, what to do an reset. since if a use system reset also same only.
can u someone suggest what to do for this reset handler issues.
regards,
srinath
2025-10-27 4:02 AM
Hello,
It's hard to help you based on the description you provided.
What board are you using? What example are you testing?
Please review How to write your question to maximize your chances to find a solution
2025-10-27 4:08 AM
Hi @mƎALLEm
stm32h45bit3 208 pin package board we designed, in this normally i have verified peripherals, clocks, etc. during testing when i try to reset the board by push button i can see m7 core resets fine no issues, while m4 core stuck in reset handler.
thus im using an nucleo board as an debugger , so reset button is pressed in nucleo board, from here via swd connector it will go to mcu respective nrst pin.
so i couldnt able to get why it is happening like this, this first time working in an dual core.
regards,
srinath
2025-10-27 4:12 AM
Still not answering all the questions: what is the example are you using for this test?
Did you test the same thing on Nucleo board and it's working?
2025-10-27 4:35 AM
thank you for the response.
nucleo board that we are using is g474 board, using this board only we are flashing the code to h7 mcu using swd.
we are not running the example code, we are running our own code,
m7 core running
2*fdcan , 3*spi, ethernet, usb , memory sharing between the cores, 2*usart, 3 timers etc,
in m4 core
tim1 6 pwm, and tim3 1 pwm and some gpio outputs,
the code is heavy only in m7 not in m4 , m4 doing only for calculations, but our problem is reset handler only, m4 stuck in reset handler.
regards,
srinath
2025-10-27 6:11 AM
Debug the code. Where is it stuck? Why is it stuck?
Perhaps get an example up and running first, then use that as a base for your program.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.